AXIS#.IL.AINSOURCE

Description

This parameter sets which analog input to use for AXIS#.IL.AINSCALE.

Value Description
0 Uses no analog input. The current command in analog torque mode is 0.
1 Uses AIN1
2 Uses AIN2

Versions

Action Version Notes
Implemented 02-00-00-000
Added value '0' to range 02-07-02-000  

General Information

Type

Read/Write

Units

N/A

Range

0 to 2
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
AXIS1.IL.AINSOURCE

500ah

15h

Unsigned8

-

-

Read/Write

No

AXIS2.IL.AINSOURCE

510ah

15h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.IL.AINSOURCE

5811

16B3

Unsigned8

Read/Write

-

AXIS2.IL.AINSOURCE

71347

116B

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.AINSOURCE

5811

Unsigned8

Read/Write

-